1/18/2012 9:55 AM | |
Joined: 10/10/2005 Last visit: 4/18/2024 Posts: 1917 Rating: (132) |
Hello, I think the suggestion of Pegaia is OK. But consider you need STEP 7 V11 with SP2 and your CPU1214C need the firmware version V2 at least. Then you can insert and program with SCL FBs and FCs. See also an example in S7-SCL, which do you can also use in STEP 7 V11 http://support.automation.siemens.com/WW/view/de/21946854 With best regards |
10/15/2013 1:27 PM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2683 Rating: (135) |
New question splitted to conceptual problem using S7-1200, SCL and pointers Best regards O_Moderator |
Follow us on