2/26/2020 3:08 AM | |
Posts: 12 Rating: (1) |
Hi bergmanu, Thanks for the replied. For your suggestion, yes. I did tried to ping for google. Best Regards. |
3/2/2020 4:57 PM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60)
|
Hello, There are some issues when installing nodes on Image V2.6.0 right now. Check out this thread. The Problem was already identified and fixed on Github, but we will have to see if we can provide a patch or a workaround for this. Which Nodes are you currently trying to install? Kind regards! |
Last edited by: Fe_lipe at: 03/02/2020 16:58:27 |
|
3/9/2020 1:50 PM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60)
|
Hello, Have you checked out this solution? The latest version of s7 nodes should work fine on V2.6.0, but you have to apply this fix before running any install command. So first flash a fresh image onto the SD card, then apply this fix provided by jan, then try installing the s7 node over the node-red palette. Kind regards! |
3/9/2020 5:25 PM | |
Joined: 11/7/2016 Last visit: 4/12/2024 Posts: 12 Rating: (0) |
Hello, I'm having the same problem. How have you solve it?? Thank you |
3/11/2020 3:41 PM | |
Joined: 11/7/2016 Last visit: 4/12/2024 Posts: 12 Rating: (0) |
Hello, Thank you for your answer. I have tried it and i still have the same problem.. |
3/11/2020 3:49 PM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60)
|
Hello, Do you have an internet connection? BR |
3/11/2020 4:52 PM | |
Joined: 11/7/2016 Last visit: 4/12/2024 Posts: 12 Rating: (0) |
Hi, I'm using a free connection. |
3/12/2020 2:10 AM | |
Posts: 12 Rating: (1) |
Hi, Did you tried to reboot and check whether the node has been added to your palette or not? If still no I have no idea ady. Because I was follow the guide attached below. Best Regards. AttachmentS7_Comunication_node-red_V1.0.pdf (267 Downloads) |
Follow us on