6/8/2007 10:46 AM | |
Posts: 62 Rating: (2) |
Hi all! I am trying to make C# application for exporting Alarm Message Archive. I had wrote application which connecting to WinCC database using Connectivity Pack v6.1 SP1. Here is sample code: [code]DataView pregled; DataColumn stupac; string sqlUpit; DataConn.DataSetHelper dsHelper; try { //DataConn.ConnectionString="Provider=WinCCOLEDBProvider.1;Catalog=" + DatabaseName + ";Data Source=" + ServerName + "\\WinCC" conn = new OleDbConnection(DataConn.ConnectionString); conn.Open(); causeData = new DataSet(); //this is SQL query - view is ALGVIEWRUS sqlUpit = "ALARMVIEW:SELECT * FROM " + "ALGVIEWRUS"; datadapter = new OleDbDataAdapter(sqlUpit, conn); //filling data adapter datadapter.Fill(causeData,"tablica"); //using DataGridView object to display data dataGridView1.DataSource = causeData.Tables[0]; conn.Close();[/code] 1. QUESTION Why when I use query like this "ALARMVIEW:SELECT DateTime FROM ALGVIEWRUS" I get error like in attachment(SelectError.jpg)? 2. QUESTION When I select all data in column DateTime I can see only date and time, but without seconds. Where is the problem? I am using WinCC v.6.0+SP4 and Connectivity Pack v6.1+SP1. Thank you for your help! AttachmentWinCCExportError.zip (117 Downloads) |
Follow us on