8/18/2014 10:41 AM | |
Joined: 5/12/2006 Last visit: 9/20/2024 Posts: 22365 Rating: (3011)
|
Hello, is no goodidea to connect the 3AC 400V power directly to the LineModule without a filter. Readthe manual for the correct line connection. You can't move or pos the axis without a correct working line module. Regards Christoph |
8/18/2014 10:56 AM | |
Posts: 55 Rating: (0) |
Hi Chris,Total agree with you!
|
8/19/2014 9:32 AM | |
Posts: 55 Rating: (0) |
Hi Chris After put in the filter, the infeed looked OK However, once we use a simple logic to control the motor the fault come up as picture attacheed We also attached the logic as well. Can you please help us find why the fault happen? Thank you very much
Attachmentattached.zip (91 Downloads) |
8/21/2014 10:57 AM | |
Posts: 55 Rating: (0) |
Hi Chirstoph, System SIMOTION C240 control S120 CU320 2 DP with module power servo03/04 my objective: how i can Sevor_03 Homing at 10deg ( or expect positon when comisioning) by Push button on HMI. that mean,before do process, operator must press Push button Home on HMI or PB home hardware. As Operator pressed Push button HOME on HMI, servo will go HOME at 10deg (HOMED) or expect position when commisioning. How to do on Axis Homing of C240. do we need Proximity Sensor wiring to C240 to detected HOMED? please give me your advice. Please take a look attached file help me! Much appriciated!
Attachmenthome.zip (125 Downloads) |
Follow us on