Industry Online Support
Technical Forum
8/17/2007 3:14 PM | |
Posts: 39 Rating: (0) |
Hi all, I'm having a problem with Connectivity Pack. I had written earlier to the forum for a Report Printing problem and was a sort of solved with Connectivity Pack. Now this is a new continuation of my earlier problems. If I access more than 4 tags in a single query then I get an error "Unhandled exception was raised. Look file 'C:\Program Files\Siemens\WinCC\Diagnose\PDLRTSEH.LOG' for details." In my project I have used the following string to access tags: sTagName="(" & "'PVA\rRP01.V';'PVA\rRP01.I';'PVA\rRP01.Hz';'PVA\rRP01.KW';'PVA\rRP01.Pf'" & ")" But if I execute the same script with 4 tags or less then I get all the tag values from the log without any problems. If I use the same string above with 4 tags then I don't have any problems at all. Eg: sTagName="(" & "'PVA\rRP01.V';'PVA\rRP01.I';'PVA\rRP01.Hz';'PVA\rRP01.KW' & ")" I have attached the script, screen shot of the error and log file with this thread. Can anyone tell me why this happens? Regards, Manju AttachmentConnectPack.zip (63 Downloads) |
8/21/2007 8:39 AM | |
Posts: 39 Rating: (0) |
Thanks Rit, |
Follow us on