8/24/2021 3:45 PM | |
Joined: 10/10/2005 Last visit: 4/18/2024 Posts: 1917 Rating: (132) |
Hello Sanza_u19, the reason could be the memory in this case. If the main memory for retentive data blocks is already full, then no more DBs are created by SFC 82 "CREA-DBL" and the error code W#16#80B2 (insufficient main memory) is returned via RET_VAL. See also the information of the FAQ: Retentivity behavior of S7-300 CPU 31x and complete devices C7-6xx with MMC With best regards |
Follow us on