1/15/2020 10:36 AM | |
Joined: 3/14/2008 Last visit: 4/18/2024 Posts: 2064 Rating: (926)
|
Hi, What CPU are you using? With older CPU's like 416/417 you need a firmware update in order to use the @CPU_RT. For example a redundant 417-4H you will need firmware :4.5 or higher. If you have a single CPU, you will need firmware: V5.0 or higher |
If I could help you, you can use the RATE button. Thank you. |
|
1/15/2020 10:54 AM | |
Joined: 12/6/2019 Last visit: 1/3/2024 Posts: 6 Rating: (0) |
I am using CPU 417-5H PN/DP with firmware version V6.0.8 |
1/15/2020 12:07 PM | |
Joined: 3/14/2008 Last visit: 4/18/2024 Posts: 2064 Rating: (926)
|
That should be good, One other cause could be that you have migrated the project without use of new functions. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on