12/10/2019 2:25 AM | |
Joined: 4/17/2018 Last visit: 2/26/2024 Posts: 262 Rating: (60) |
Hello, As I heard the new feature on tia portal v16 opc ua on s7-1200 v4.4. So I upgraded firmware of my cpu 1214 dc/dc/dc and I tried to test this new feature (opc ua server). I maked all steps like s7-1500 and I used UaExpert as opc ua client simulator. after making connection with opc server (s7-1200) I don't find variables for monitoring but when I make same steps with s7-1500 I can read/write variables as you see in attachment. So what is the purpose of activating opc ua server in s7-1200 if we cannot monitor data? Attachmentpictures.pdf (284 Downloads) |
12/10/2019 7:52 AM | |
Joined: 5/12/2006 Last visit: 3/27/2024 Posts: 22162 Rating: (2962) |
Hello, have you configure a OPC Server Interface in the project three of the S7-1200? (Subfolder OPC UA_Communication on the PLC project three)
please take a look in the Systemmanul for Version V4.4 to understand how the OPC_UA work on the S7-1200 https://support.industry.siemens.com/cs/ww/en/view/109772940 Regards Christoph |
Last edited by: ChristophD at: 12/10/2019 07:53:59 |
|
This contribution was helpful to1 thankful Users |
12/10/2019 8:43 AM | |
Joined: 4/17/2018 Last visit: 2/26/2024 Posts: 262 Rating: (60) |
Thank you for your help, I miss opc ua server interface configuration, I will try it. Best regards |
3/18/2020 2:24 AM | |
Joined: 7/25/2017 Last visit: 3/27/2024 Posts: 291 Rating: (43) |
Hello Med_selmi! Did ChristophD's advice resolve the issue? Cheers |
Follow us on