2/3/2016 1:46 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1047) |
hi, try to reinitialize your interfaces. following FAQ will help: How do you assign the parameters of the PG/PC interface in general and what is the remedy if the device driver cannot be selected or is not visible?hope this helps, regards, |
FCK WAR! |
|
2/3/2016 1:47 PM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (813) |
Hello, pls look at attachment, there is BATCH file what yoiu need run. For first look in to file internaly what it do to understand. This Siemens service update Interfaces. AttachmentPG_Interfaces.zip (538 Downloads) |
With best regards... |
|
2/3/2016 4:22 PM | |
Joined: 6/5/2007 Last visit: 2/28/2024 Posts: 11 Rating: (0) |
Thanks for the reaction, but it don't work |
2/4/2016 8:37 AM | |
Joined: 5/12/2006 Last visit: 3/28/2024 Posts: 22162 Rating: (2962)
|
Hello, the PG/PC Interface in the control Panel is from the component Simatic Device Drivers. You can search the registry if any Siemens Shared Component is allready installed after you uninstall the Software. Depends on which SW you had installed an then uninstall Registry settings and files on the System are present after uninstall. here 2 FAQ's fore a complete uninstall of Siemens SW: https://support.industry.siemens.com/cs/de/en/view/189025 https://support.industry.siemens.com/cs/de/en/view/76325723 Regards Christoph |
Follow us on