12/1/2011 8:47 AM | |
Joined: 10/19/2011 Last visit: 5/3/2024 Posts: 31 Rating: (1) |
Hello. Could you help me with my problem please. I have got machine with Sinumerik 810D system. It works but not in appropriate way. The spindle override works in all modes except an AUTO mode. I have to fix it. As I understood it works through the FC19 block but I can't realize how this block works. I attach my FC19 block (source code). What is wrong in it? And one more question. Where the signal mst_ein01 is formed in standart block FC19 from SINUMERIK Toolbox? In place of code below: ///NETZWERK Eingang L DB8.DBW 90; DEC 1; T #achs_db; //Lokal machen L DB5.DBW 20; //Grundprogrammparameter maximale Anzahl der BAGs T #max_bag; L DBW 22; //Grundprogrammparameter maximale Anzahl der Kanaele T #max_kan; L DBW 24; //Grundprogrammparameter maximale Anzahl Achsen + Spindeln T #max_axe; //Umladen GP-Parameter in lokale Variablen LAR2 P#mst_ein01; //Adresse mst_ein laden (Var_temp Datum) !!! //AR2 wird im gesamten Baustein als Zeiger //verwendet LAR1 DB7.DBD 4; //Grundprogrammparameter bereichsuebergreifende Adresse der MST Where should we take var_temp #mst_ein01 that write it to AR2? It haven't assigned yet because it is beginning of block. Am I right or not? AttachmentFC19.zip (68 Downloads) |
12/2/2011 2:57 AM | |
Posts: 10 Rating: (0) |
Does not need to modify the FC19, need only in the automatic mode of spindle PLC interface signal DB3 *. DBX1.7 does not activate it. |
12/5/2011 11:52 AM | |
Joined: 10/19/2011 Last visit: 5/3/2024 Posts: 31 Rating: (1) |
Bits DB*.DBX1.7 are setted in my FC30 (at the bottom of the block)
AttachmentFC30.zip (63 Downloads) |
Follow us on