4/23/2012 4:22 PM | |
Posts: 59 Rating: (1) |
Hello friends, I have a problem with the program mentioned in the "subject" tab. After I start de program a error message appears(see attach) and the program closes (in about 1 min after start of program). If anyone has encontered this problem please reply. Thank you. AttachmentEroare din prog.zip (441 Downloads) |
Last edited by: O_Moderator at: 4/24/2012 12:27 PMattachment edited to "real zip-file" |
|
4/23/2012 8:31 PM | |
Joined: 2/16/2011 Last visit: 4/4/2024 Posts: 229 Rating: (27) |
Hello; Did you try to reinstall the application. Regards
|
Gabriel de Oliveira |
|
4/24/2012 7:22 AM | |
Posts: 59 Rating: (1) |
I had some errors during installation but i managed to pass them. At the end of the install process the program says "An error occurred during setup". In attach you will find the error screens.
AttachmentS7_1200.zip (433 Downloads) |
Last edited by: O_Moderator at: 4/24/2012 12:28 PMattachment edited to "real zip-file" |
|
4/24/2012 7:28 AM | |
Posts: 1064 Rating: (72) |
Sounds like you need to re-install after reading the file indicated in the error log and following the instructions |
4/24/2012 7:32 AM | |
Posts: 59 Rating: (1) |
Other suggestions?(the error log is huge) |
Last edited by: Krsh at: 4/24/2012 7:44 AM |
|
4/24/2012 10:49 AM | |
Posts: 59 Rating: (1) |
Change the file extension from ".zip" to ".rar" extract and it will work. |
4/24/2012 12:29 PM |
|
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2683 Rating: (135) |
Now it should work without changing the file extension |
4/24/2012 12:34 PM |
|
Posts: 59 Rating: (1) |
It should also be posible to upload .rar files not only . zip files! |
Follow us on