Industry Online Support
Technical Forum
1/1/2011 11:16 PM | |
Joined: 6/4/2008 Last visit: 4/23/2024 Posts: 1481 Rating: (322)
|
Hi, first, make sure the drive is disabled, it must not be in operation mode, or the parameters may not be changeable. Also, make sure P0003 = 3. Please see the attached function diagram showing the Digital Outputs, literally, you would make the parameters for the new Digital Output match those from Digital output 2. For example, if you wanted to use Digout3 instead, then you would make P733.1 = P732.1 and you would wire to pins 24 and 25 instead. (P748 is a binary representation of the inversion of the three digital outputs, for example, if you wanted to invert all three digital outputs, you would enter a value of 7 which is 111, default is 0) Hope this helps. Cheers, Graeme
AttachmentMM440_DigOut.pdf (80 Downloads) |
Follow us on