4/25/2013 11:19 AM | |
Joined: 10/10/2005 Last visit: 4/18/2024 Posts: 1917 Rating: (132) |
Hello Peed Off User, it seems as if that you have a lot of exasperation with the TIA Portal in the last time. But as things are now the STEP 7 (TIA Portal) with version V12 runs under Windows 7 very good. The GSM can only 9600 bit/s and is adequate for small applications. The performance is essentially dependent of the modems. In TIA Portal allows the CP1242-7 for the S7-1200 to communicate as a GPRS station with a central station or a remote network via the GSM network. An extensive description you will find also in the online help. The program code of STEP 7 (TIA Portal) is like as by STEP 7 V5.5. There are also a lot of new functions in V12 and consists the new high-performance S7-1500. But in the foreground is the symbolic programming method in STEP 7 (TIA Portal) and you can use the function "Drag&Drop" in the most of the applications. See also the informations and news of the sides by Siemens in the internet "TIA Portal - The new Automation Framework for SIMATIC" under the following link: http://support.automation.siemens.com/WW/view/en/65601780 With best regards |
Follow us on