6/21/2018 1:00 PM | |
Posts: 14 Rating: (0) |
Hello guys As you know in simatic manager we easily adjusted TOD interrupt setting by clicking on cpu and going to interrupt part for example we want to stop plc in the first day of every year at 07:00 AM o'clock but 1-fist problem: we can only set execution and start time as Date not Time [snip] 2-second problem: also we have only OB10 ... as u see in attach2 [snip] 3-third problem: when we use "SET_TINT" SFB for interrupt .. we don't see the setting for "time of day" 4-forth problem: What is the type of SDT (START TIME) and how can i set a date and time for that??? thanks ---------------------------------------------------- I'm sorry to edit too Photos were removed several times ... now img are existing as attach
Attachmentimg 01 02.zip (154 Downloads) |
Last edited by: hdportal at: 6/21/2018 1:01:05 PMLast edited by: hdportal at: 6/21/2018 1:02:18 PMLast edited by: Jen_Moderator at: 6/22/2018 9:18:49 AMDeleted links and added files as an attachment. Last edited by: hdportal at: 6/22/2018 10:55:49 AMLast edited by: hdportal at: 6/22/2018 10:57:15 AMLast edited by: hdportal at: 6/22/2018 11:48:06 AMLast edited by: Jen_Moderator at: 6/25/2018 8:18:52 AMDeleted links, because files are added as an attachment. |
|
6/21/2018 4:32 PM | |
Posts: 14 Rating: (0) |
Yeah Thanks my friend second problem solved and now i know we have setting time but i don't know how to set time? we cant set the time from clicking on cpu and going to interrupt setting [snip] we cant set time in SFB SET_TINT directly [snip] we cant set time from memory area and change default value for SDT [snip] we cant use constant memory area for SDT [snip] so what can i do? ---------------------------------------------------- I'm sorry to edit too Photos were removed several times ... now img are existing as attach Attachmentimg 01 02 03 04.zip (110 Downloads) |
Last edited by: hdportal at: 6/21/2018 4:34:11 PMLast edited by: hdportal at: 6/21/2018 5:43:48 PMLast edited by: hdportal at: 6/21/2018 10:54:39 PMLast edited by: Jen_Moderator at: 6/22/2018 9:22:14 AMDeleted links and added files as an attachment. Last edited by: hdportal at: 6/22/2018 11:14:15 AMLast edited by: hdportal at: 6/22/2018 11:15:11 AMLast edited by: hdportal at: 6/22/2018 11:45:08 AMLast edited by: Jen_Moderator at: 6/25/2018 8:19:42 AMDeleted links, because files are added as an attachment. |
|
6/22/2018 11:54 AM | |
Posts: 14 Rating: (0) |
Nooooooooooooo Not solved |
6/22/2018 5:06 PM | |
Posts: 14 Rating: (0) |
"" So much negativity and zero creativity. "" Hey stop it man """Put the instruction in an FB and call it from OB1""" I tested before ... did not work In FB i use ""STATIC and IN"" memory area for SDT because i had temp and constant memory in OB1 but did not work again I could set a time for sdt in STAT and IN but nothing happened in that time """use the F1-Help in TIA portal a little bit on your own""" Yes sure ... I use F1 all time but in this fucking situation i don't know anything I know u are better but this cant be the reason you judge this way This problem has made me angry Attachmentpic.zip (100 Downloads) |
6/23/2018 11:12 AM | |
Posts: 14 Rating: (0) |
Dear mopS04 and huggy_d1 Thank you very much for the help I was finally able to conclude We should set parameters in SET_TINT then activate with ACT_TINT The arrangement of these two is very important Some important points that friends have explained are in the pictures F1_Help Attachment01 02 03 04 05.zip (119 Downloads) |
Follow us on