6/19/2009 10:44 AM | |
Joined: 1/8/2009 Last visit: 4/20/2020 Posts: 5 Rating: (0) |
Hello to all, I have been struggling for sometime with this problem. When I start the Runtime and click on the tab that contains a picture in particular, the following error comes up: Unhandled exception was raised. Look file "C:\XXXXXXX\PDLRTSEH.LOG" As I look at the file, which I have attached, and from what I can gather there seems to be an error with a .dll file; which I have also attached. The curious thing is that this same project is running on a different machine without problems, I still need to check once again what SW versions are installed in the other machine but they are the same. I have PCS 7 V7.0 SP1, and WinCC V6.2 SP2 running Thanks in advance for the help. David Attachmentfiles.zip (111 Downloads) |
6/23/2009 3:25 AM | |
Posts: 1275 Rating: (123)
|
Hi Dave, The access violation errors I've seen are usually linked to a script trying to access a file / folder it's not allowed to, or that doesn't exist. Check these previous threads, for instance:1,2,3,4. You can find other similar threads by searching the forum... I've also seen cases,such as this, where an incompatible software was installed, causing instabillity. Run your application under APDIAG, to check for scripting errors... also check the error logs. Best regards, Danielle
|
Follow us on