3/18/2013 9:40 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927) |
Mark is correct, however you have to do an additional step in wincc explorer: In Wincc explorer, goto tag management and select the connection where you compiled the os (prefer TCP/IP). On the TCP/IP connection, right click and click: System parameters. In there, on the last tab you have to select the PLCSIM.TCP/IP connection (or other depends on your chosen connection). Now Wincc will communicate... |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on