2/7/2018 12:57 PM | |
Posts: 1 Rating: (0) |
Hi, I have problems with the communication of the step 7 Micro / WIN program. Before I had a computer with xp i with a serial port and everything went well, now I have changed the computer for a Windows 10 operating system and I do not have a serial port, I do it with a usb to serial port converter. I installed the Micro / WIN and it works well so I can not connect to the S7-200 since I do not see the PC / PPI cable anywhere. I would appreciate answer Thank you ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 2/7/2018 3:08:58 PMNew subject after splitting |
|