3/30/2014 11:37 AM | |
Joined: 11/21/2007 Last visit: 9/25/2024 Posts: 2325 Rating: (308) |
Hello Friends We are presently in an enviornment in which Both Profibus and Profinet networks are in wide use. Users are often confused between the two. With this Post, I am trying to consolidate some of the information available in Siemens Support as well as other Websites regarding Profibus and Profinet. Here are a few links : 1. PROFIBUS ( Wikipedia) 2. PROFINET ( Wikipedia ) 3. PROFIBUS + PROFINET - Strategic Overview - A White Paper 4. Introduction to PROFIBUS and PROFINET ( profibus.com ) ( Pl See attachment below if link does not work ) 5. SIMATIC PROFINET System Description 6. From PROFIBUS DP to PROFINET IO and From PROFIBUS to PROFINET 7. Comparison of the terms of PROFIBUS and PROFINET I hope that these documents will help users to understand both types of networks and selecting the right network for their requirements Cheers Navnag AttachmentIntroduction_to_PROFIBUS_&_PROFINET.pdf (723 Downloads) |
Last edited by: Navnag at: 3/30/2014 5:26 PMWikipedia Links Corrected There is no such thing as the last bug in a program |
|
This contribution was helpful to12 thankful Users |
3/30/2014 5:14 PM | |
Joined: 9/27/2006 Last visit: 9/25/2024 Posts: 12283 Rating: (2685) |
Hello S7 Automan; These links will provide you the information that Navnag intended originally: http://en.wikipedia.org/wiki/Profibus http://en.wikipedia.org/wiki/PROFINET Hope this helps, Daniel Chartier |
This contribution was helpful to2 thankful Users |
4/1/2014 11:25 AM | |
Posts: 9 Rating: (0) |
thank you very much for this document |
This contribution was helpful to1 thankful Users |
5/23/2014 8:26 AM | |
Joined: 11/21/2007 Last visit: 9/25/2024 Posts: 2325 Rating: (308) |
Hello Friends Here is another nice document I stumbled upon regarding Profibus & Profinet. ( Pl see attachment ) Here is another interesting take on : Profibus Vs Profinet. Although, I must admit that I do not agree fully with all the points made in this article. Call me old fashioned, but I am still a fan of profibus - for communication in Field area, whileI have no issues in using profinet for communication within control rooms. Cheers Navnag AttachmentGuide to efficient changeover from Profibus to Profinet.pdf (549 Downloads) |
Last edited by: Navnag at: 5/23/2014 8:26 AMThere is no such thing as the last bug in a program |
|
5/24/2014 5:38 PM | |
Joined: 1/17/2010 Last visit: 8/21/2024 Posts: 77 Rating: (5) |
Havea look on the below links for profibus and profinet netwroks. http://support.automation.siemens.com/WW/view/en/32425069 http://support.automation.siemens.com/WW/view/en/32425069 http://cmsapps.sea.siemens.com/sitrain/wbt/Profibus/start.htm Good luck |
Last edited by: mostref at: 5/24/2014 5:40 PM |
|
This contribution was helpful to3 thankful Users |
Follow us on