Industry Online Support
Technical Forum
7/3/2006 9:20 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (315)
|
[quote user="erenakc"]I have midimaster drive (6SE3122-4DG40). I want to connect with s7-416 2 DP but ı dont have gsd files.If anybody have gsd files and samle project, can anybody send... Hi Erenakc, Please find the GSD-files under the link: PROFIBUS GSD files : DRIVES Handbook OPERATING INSTRUCTIONS FOR MICROMASTER ECO & MIDIMASTER ECO Communication Board Handbook PROFIBUS-DP Communications Module CB15/CB155 I have no example for the communication, but you can choose a PPO-type and then have to find the bits and bytes that are in use for that. [;)] |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on