Industry Online Support
Technical Forum
7/9/2013 3:42 PM | |
Joined: 10/11/2006 Last visit: 9/18/2024 Posts: 5906 Rating: (804)
|
Hello, For the configuration of such a communication you should use the mask IF1: telegramas PZD PROFIdrive. There you select the order of your drive objects and you select the necessary telegram for each object. In the S7-1200 we would create the Profibus / Profinet communication using the GSD / GSDXML file of the Sinamics DCM. It is possible that you have to install these files at first in the TIA Portal and then you can create the communication also in TIA Portal. Just have a look on the following application example - its no DCM but its also using a GSD / GSDXML file for the communication: http://support.automation.siemens.com/WW/view/en/56749384 |
With best regards, |
|