2/17/2010 12:52 PM | |
Joined: 2/24/2009 Last visit: 3/4/2024 Posts: 26 Rating: (0) |
Hello, I need to connect Schneider Electric VFD ATV61 DPV1 to S7-313C-2DP controller via Profibus and because I'm beginner and I am a bit confused from what I read in Schneider's manual (in enclosure), I would like to ask questions below: 1. Should I use DIRECT or INDIRECT access mode mentioned in enclosure? I saw in some manual, that I should be able to use direct access on my CPU. But when I choose to change CPU type I could run into trouble - CPU15-2DP does not support it for example...(A5E00105475-06 manual page A6 - 222) ? 2. Should I use SFB52/53 or SFC58/59 as it is on page 32 of enclosed "ProfibusDPv1" manual? Which way is standard? I just want to control the VFD (command word) and listen to status word, but it is possible somebody will ask me to change parameters of VFD online. Thank You Very Much Andrej AttachmentProfibusDPv1.pdf (346 Downloads) |
Last edited by: andrej5 at: 2/17/2010 12:53 PM |
|
2/17/2010 6:25 PM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181)
|
Hello Andrej, Perhaps follow discussion would helps a little - Altivar71 and CPU315-2DP using Profibus Best regards, Hristo Mihalev |
Follow us on