2/9/2010 5:35 PM | |
Posts: 95 Rating: (0) |
Hello I have a customer with a hardware configuration depicted in the attachedp PDF. First Question, the hardware configuration includes all devices shown, but physically two slaves are not there (nodes 27 and 28). This leads to a continuous BF light on the CPU (400). Will this always be the case or can the scanning of the devices be disabled without removing them from the HW Config? These are future devices. [schnippschnapp] John AttachmentVisio-Network Diagram Rev D_LWH.pdf (45 Downloads) |
Last edited by: O_Moderator at: 2/10/2010 12:18 PMsecond question is in the following thread /tf/WW/en/Posts/40069#top |
|
Follow us on