11/25/2019 4:31 PM | |
Joined: 9/27/2006 Last visit: 9/22/2024 Posts: 12282 Rating: (2685) |
Hello Alexander; With so few details on your installation, it is difficult to provide useful replies to your situation. It might be helpful to show us the contents of the CPU's diagnostic buffer; use the Save AS... button on the diagnostic buffer page to transfer all messages to a text file that can be attached to your posts. One thing I would like to look at is the timing of the station losses; if they are lost at the exact same time, it could be either (just a few possibilities): - a power problem on the Profibus nodes(if they are all powered from the same source and it becomes unstable), - a termination problem; both end stations (the first and last physical nodes on your network) must have termination resistors set to ON and must remain powered at all times to activate the termination circuit. if the termination is lost (power is removed from the station) reflections appear on the network and the CPU master can be submerged by erroneous messages that overwhelm it, and the network fails. - EMC issues, where the Profibus cable is too close to an electric field, such as a motor turning on; this may induce voltage on the network connections and make it fails also. See if any of these ideas help you, check all cable runs and verify every Profibus connectior for adequate wiring (validate especially the shield connection, proper grounding is imperative). And see if the links below can be helpful. TOP 5 REASONS YOUR PROFIBUS NETWORK FAILED https://us.profinet.com/top-5-reasons-your-profibus-network-failed/ A short guide to addressing EMC on PROFIBUS – Procentec https://procentec.com/about/news/2016/a-short-guide-to-addressing-emc-on-profibus/ Tips for trouble shooting on the PROFIBUS-DP | SMAR http://www.smar.com/en/technical-article/tips-for-trouble-shooting-on-the-profibus-dp Installation guides- Profibus.com Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 11/25/2019 16:33:39 |
|
This contribution was helpful to2 thankful Users |
12/11/2019 9:08 AM | |
Joined: 4/13/2013 Last visit: 9/15/2021 Posts: 14 Rating: (1) |
Hello Daniel, Thank you for the help. I would not like to believe it is a installation issue since it affects SIMOCODES on 4 different PLCs each with its own network and affected at a more similar interval. We do have parts of the installation that we should still bring to conformance with the guidelines. The problem has since not happened the past two weeks, thus I don't have CPU diagnostics log yet. Yes, we do have a number of erroneous messages coming in on some of the units which we are also trying to attend to. But this messages are mainly coming from the field PA devices. Yes the SIMOCODES are powered from the same power source however there is a time difference of ±10 minutes between each PLC when the SIMOCODES goes down. |
Follow us on