4/15/2020 11:27 AM | |
Posts: 8 Rating: (0) |
HI, we have the PROFIBUS based S7-315 system as shown in the attached file. that system was working properly for years ago " except it once subjected to PROFIBUS cable failure and after replacing it the problem was fixed" NOW the SF LED in PLC is always on and the BF LED is flashing. after seeing the PLC Buffer we do the next a step by step: 1. Replace the standard PROFIBUS cable with a PROFIBUS Festoon cable so that it can afford bendings like bendings founded in crane systems. 2. Replace all the PROFIBUS connectors with a new one. 3. Replace the ET-200M interface modules with a new one having the same version. 4. Replace the RS485 Repeater. 5. even we replace the CPU. 6. re download the Hardware config and BLOCKS. 7. Review all the configuration including terminal resistors, Addresses & Baud rate in all the system the problem is still exist "SF LED is always on and the BF LED is flashing" !!! AttachmentDiag&net.zip (64 Downloads) |
4/15/2020 9:05 PM | |
Posts: 8 Rating: (0) |
the attached pics show the all the SYSTEM modules & hardware the addresses PIW 256 & 260 are for RFID READER MOBY D ASM 475
Attachmentpics.zip (53 Downloads) |
Follow us on