4/26/2017 2:57 PM | |
Joined: 9/27/2006 Last visit: 3/28/2024 Posts: 12249 Rating: (2660) |
Hello Masoodes; Have a look at this screenshot from Siemens Product Support, for the IM 153-4 PN IO interface module (for ET 200M). You would need to remove the IM 153-1 from your remote profibus IO rack, replace it with the Im 153-4, connect your radio and the new IM with Ethernet cable, and configure a Profinet network in your project connecting to the IM 153-4. For basic information on creating a Profinet connection (including setting an IP address and a Name for the Profinet IO module), see here (sections 5.5 and 5.6 of the Profinet manual); PROFINET System Description - SiemensHope this helps, Daniel Chartier |
This contribution was helpful to2 thankful Users |
4/27/2017 5:53 AM | |
Joined: 9/8/2015 Last visit: 3/16/2024 Posts: 109 Rating: (1) |
Thank you, your answer was useful |
Follow us on