12/16/2009 9:49 PM | |
Joined: 9/27/2006 Last visit: 5/13/2024 Posts: 12257 Rating: (2668) |
Hello chimpu; One solution we looked at for a project was the Prolinx Profibus Wireless Gateways, from Prosoft Technologies. They are described here: http://www.prosoft-technology.com/content/view/full/8664 More information is available on the links on the right of the page. Of course you will have to take line-of-site distances and antennas into consideration, as well as allowaed frquencies in your part of the world. Prosoft has an excellent support record, and they could help you configure the application. I have modified your initial diagram to show how you could use it with the Prolinx Gateways. Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
12/17/2009 8:51 AM | |
Joined: 12/9/2009 Last visit: 4/18/2024 Posts: 156 Rating: (11) |
Hello, I also would prefer optical cable. There are the PROFIBUS OLM with electrical interface (RS485) and optical interface (BFOC). For exampleyou can use this components to overcome the distance between S7 station and ET 200M with optical cable. AttachmentMN_OLMV4_0.zip (57 Downloads) |
12/17/2009 8:57 AM | |
Posts: 378 Rating: (47) |
And here is the english version of the manual published by little_holmes best regards bilao AttachmentMN_OLMV4_76.pdf (47 Downloads) |
12/17/2009 3:30 PM | |
Posts: 691 Rating: (36) |
Will it be converted automatically I mean to say ; I need not set any configuration for the Antenna |
Follow us on