Industry Online Support
Technical Forum
5/12/2010 6:20 PM | |
Joined: 3/21/2006 Last visit: 4/4/2024 Posts: 10228 Rating: (1181)
|
Hello no, Seems OK. And if you have some troubles with settings look at How do you program the communication blocks FB63 "TSEND", FB64 "TRCV", FB65 "TCON" and FB66 "TDISCON" in order to use the TCP protocol for data exchange via the integrated Industrial Ethernet interface of an S7-300 or S7-400 CPU? Best regards, Hristo Mihalev |
5/12/2010 6:39 PM | |
Posts: 3093 Rating: (322) |
Hello ne, yes, you are right. Regards, Kaulquappe |
5/12/2010 9:23 PM | |
Posts: 18 Rating: (0) |
Hristo Mihalev and Kaulquappe - many thanks to you both! |