10/31/2013 4:54 PM | |
Posts: 9 Rating: (0) |
I have the same problem on my PLC. My colegue is using integrated PN port on CPU and FB10 “PZD_G120_Tel_352” is working fine. On my PLC I am using CP 343-1 and the block didn't work. On this link I found that with CP 343-1 you must use FC11 and FC12 (mandatory), so I made changes to FB10 “PZD_G120_Tel_352”. https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&objId=61450312&objAction=csOpen&nodeid4=34677186&cspltfrm=0&cssw=0&csbinh=8&lang=en&siteid=csius&aktprim=4&extranet=standard&viewreg=WW Now it calls FC11 and FC12 instead SFC14 and SFC 15. But I still can't get telegram from G120. Error code from FC11 and FC12 are 16#8183 which can be anything. Profinet connection is OK and online status of G120 is showing that VFD is sending data ( 353 ). I tried almost everything regarding the parameters for FC11 and FC12, but nothing. I belive that problem is in CP 343-1. Using web based diag on CP, I found that Profinet IO program blocks are not running. Maybe this can be the problem. If you resolve this problem, please give feedback regarding this issue. I can send you more info if this doesn't help. Regards AttachmentFB10 source code.pdf (274 Downloads) |
10/31/2013 4:58 PM | |
Posts: 9 Rating: (0) |
CP 343-1 error |
11/1/2013 3:29 PM | |
Posts: 17 Rating: (1) |
Dear: thank you for your information. At the moment, we are using PN without CP 343-1. We are waiting for more information and help. Regards. Francis. |
11/18/2020 3:59 PM | |
Joined: 9/24/2010 Last visit: 4/21/2024 Posts: 118 Rating: (10) |
You can read out more information at here: https://support.industry.siemens.com/cs/ww/en/view/26558253 And you can reference my project with SIMATIC Manager for PLC and TIA Portal for drives. Attachment1. CP343 Advanced vs G120.zip (265 Downloads) |
Last edited by: Jen_Moderator at: 11/19/2020 09:22:05Optimized link. Mechatronic Center |
|
3/3/2021 3:49 PM | |
Joined: 1/1/2017 Last visit: 5/9/2024 Posts: 329 Rating: (11) |
Thank You! Regards OmKris |
Follow us on