2/12/2016 8:55 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1050) |
Hi Dave, Failsafe modules works otherwise than normal modules. The DO switching P and M. So you have to measure between P and M of the same channel. It also can detect wire break with this method. So if there is no current, when you turn DO on It would switch off again. The DI have 3 ways to config. 1-channel; 2-channel equivalent; 2-channel, non-equivalent Default setting is 2-channel equivalent. therefore the 2 channel have to turn true between the parametrized Discrepancy time. For more information see the manual of ET200s Distributed IO Sytem SIMATIC Distributed I/O System Fail-Safe Engineering ET 200S Distributed I/O SystemAll available modules are particulary described with application-diagrams in chapter 7. hope this helps, regards, |
FCK WAR! |
|
2/12/2016 9:01 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1050) |
hi David, I would suggest to get more rudimentary information about Distributed Safety. The DI only appear in Safty programm. This should be called in a contiuous time cycle in a cyclic-interupt-OB, e.g. OB35. Have a look in this manual: SIMATIC Industrial Software S7 Distributed Safety - configuring and programminghope this helps, regards |
FCK WAR! |
|
This contribution was helpful to1 thankful Users |
2/12/2016 9:59 AM | |
Posts: 767 Rating: (69) |
Thank you mopS04, hat was really helpful. It seems to be more complicated than I thought. Are you, by any chance, aware of any sort of example that I can go through to understand how it works? Regards, Dave
|
2/12/2016 10:33 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1050) |
hi Dave, recently I have no one that I can share. But Siemens has some. Follow this link, there you have to open a Service Request to get a application sample, directly from Siemens. Burner application example for Distributed Safety and F Systemshope this helps,regards, |
FCK WAR! |
|
This contribution was helpful to1 thankful Users |
Follow us on