11/17/2021 7:51 PM | |
Joined: 1/24/2021 Last visit: 3/31/2024 Posts: 1 Rating: (0) |
HELOO kindly help me in program of load shell in logo , load shell 120kg max, so i connect the load shell in a load shell controller & the controller 4 to 20 ma feed back to logo . my application is after 10kg the the do is stop, kindly help me for scaling ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/18/2021 09:18:29New subject after splitting |
|