4/17/2013 5:51 PM | |
Posts: 391 Rating: (50)
|
Hi, you can try with "program selection via job lists", please check 10.4.5 Creating a Joblist https://www.automation.siemens.com/doconweb/pdf/SINUMERIK_SINAMICS_02_2012_E/BHUsl.pdf?p=232#page=232&view=FitBH,0&pagemode=none 5.5.2 Program selection via lists http://www.automation.siemens.com/doconweb/pdf/SINUMERIK_SINAMICS_02_2012_E/828D_LH1.pdf?p=491#page=491&view=FitBH,0&pagemode=none or, you can do that by yourself, for example: create a MAIN.MPF program that loops, continuously checking a R parameter. When R[x]=1, the MAIN.MPF calls your first program, when R[x]=2 MAIN.MPF calls your second program and so on. At the end of the loop set R[x]=0 and then restart the loop. in the PLC you write the R[x] parameter according to the input coming from the external selector. Please check DB1200 in the 828D documentation and 14.6.1 Read/write NC variables https://www.automation.siemens.com/doconweb/pdf/SINUMERIK_SINAMICS_02_2012_E/FB1sl.pdf?p=1153#page=1153&view=FitBH,0&pagemode=none |
This contribution was helpful to1 thankful Users |
10/23/2013 8:33 AM | |
Posts: 664 Rating: (17) |
Hai MBA, Can you able to give a sample PLC program for Progrm selection.. Thanks&Regards, Raj |
12/5/2013 2:28 PM | |
Posts: 664 Rating: (17) |
Hai, Anyone having answer to help me.. Thanks&Regards, Raj |
12/9/2013 9:17 AM | |
Posts: 391 Rating: (50)
|
there is no more MD
|
12/10/2013 1:29 PM | |
Posts: 664 Rating: (17) |
Hai APC Tech Team, I am attaching the screen shots of Program list,Parameter set and PLC program.. Thanks&Regards, Raj |
12/10/2013 1:30 PM | |
Posts: 664 Rating: (17) |
PLC program |
12/10/2013 1:31 PM | |
Posts: 664 Rating: (17) |
Parameter set.. |
Follow us on