6/23/2014 2:23 PM | |
Posts: 47 Rating: (0) |
Hello, I’ve got a programming problème and I hope you will be able to help me. I want to know during how many time an engine of my company is running. And this, between 3 différents ranges of hours: 22h-6h, 6h-14h and 14h to 22h. For that, I wrote the program in attachment. The problem is, when I try to load the block into the automate S7-300 that I have, the automate says: "The block does not exist Also, when I check the diagnostic buffer it is telling me that I have an illegal command in the block, FB number: 70, Module adresse: 80, Opérating mode: configuration in RUN (I am in mode Run-P), Internal error, Event entering state. As I am pretty new with programmation, I wanted to know if you could detect where does the problem comes from. Finnally, I deleted the block which made the error, but the statement that there is a programming error stays (the SF red led on the automate is ON) I would like to know how to clear the problem to make the SF light turned off. I want to add that I never load the FB 70 in the OB1 so the program is running fine but with the SF light ON. Sorry if I ask a lot these days, but I have no one else to ask. Thank you in advance for your time. Attachmentprogramme.pdf (73 Downloads) |
This contribution was helpful to1 thankful Users |
6/23/2014 3:26 PM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello lolo1234, If you still have the CPU 6ES7 315-2AF02, in segment 2 you have FP M 281.0, try with under M255.7
|
6/23/2014 4:44 PM | |
Posts: 47 Rating: (0) |
Well here is my diagnosis buffer in attachment. All the problems that I have happened with tests that I made on différent function blocks. Here you can see the FB 14 but all the other problèms are exactly the same exept that the FB changes. And all the FB shows there were deleted. So I don't really know what to do. Attachmenterrors.pdf (67 Downloads) |
Follow us on