11/25/2011 12:31 PM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365) |
Dear vasso123 , Selection of programming language depends on the task you want to implement.If the task are mainly concerned with binary signal "Ladder" and "FBD" would be the proper choice.For more complex processing tasks which needs complex variables and indirect addressing ,you should use "STL" which is a assembly like programming language. For very complex control tasks, you have option of using "SCL" which is a high level programming language and it is similar to PASCAL. Also check the followings: The SIMATIC Manager The S7 Architecture The Basic Languages LAD, FBD, STL The High-Level Language S7-SCL Best regards, Hamid Hosseini |
11/25/2011 12:41 PM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365) |
Dear vasso123, For SCL check the following manual: http://support.automation.siemens.com/WW/view/en/18735131 http://support.automation.siemens.com/WW/view/en/5581793 http://support.automation.siemens.com/WW/view/en/1137188 Best regards, Hamid Hosseini |
This contribution was helpful to1 thankful Users |
11/26/2011 5:56 PM | |
Posts: 327 Rating: (28) |
Greetings There is also VIPA. It says here that their software can be used for programming Siemens hardware:http://www.vipa.de/en/products/software/programming-software/ Best regards
|
Last edited by: fbelic at: 11/26/2011 5:58 PM |
|
Follow us on