7/14/2013 10:39 AM | |
Posts: 9 Rating: (0) |
Dear all, I want to know if SIMATIC STEP 7 TIA Version 12 can be used to configure and program S7400H (S7412 5H system Bundle) Thanks in advance, |
7/14/2013 11:27 AM | |
Posts: 559 Rating: (87) |
No it is not possible. You have to go for Simatic manager only. Please look at the below link. /tf/WW/en/Posts/58509 |
7/14/2013 12:00 PM | |
Joined: 12/1/2009 Last visit: 9/5/2024 Posts: 672 Rating: (147) |
Dear AsAPLC, everything takes it own time. The redundant S7-400H CPU's are always the last when it comes to innovations (in example see Profinet support). They will be integrated intothe TIAwithoutany doubt but when exactly I don't know. Maybe somebody here knows aschedule for that. Unitl that time, as SolutionFinderalready mentioned, you will Need to go the "old fashion" way with standard STEP7. The document in the link above shows a schedule for PCS7 and not TIA. As per my knowledge PCS7 is currentlyrunningparallel to TIA (Integration into TIA ???). Regards. |
Give us your feedback and show us your respect! |
|
This contribution was helpful to1 thankful Users |
7/15/2013 10:01 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Yes, Sterp7 5.5 is "good" foret200sp. Of course update Step7 to the last SP. In this case SP3 (Service Pack 3 for STEP 7 V5.5). Best regards, Hristo Mihalev
|
Follow us on