6/1/2011 1:23 PM | |
Joined: 1/24/2008 Last visit: 5/28/2024 Posts: 30 Rating: (1) |
I have a project created in TIA Portal V10.5. The project uses two PLCs s7-1200 and one HMI KTP600. When I tried to open the project with the TIA Portal V11 it gives the following error, as you can see in the attached file: Error occurred while converting the type 'CodeBlockData' (model type 'Siemens.Simatic.PlcLanguages.Model.CodeBlockData') Any suggestion? Thank you. Attachmenthome.pdf (690 Downloads) |
6/1/2011 1:59 PM | |
Joined: 4/24/2006 Last visit: 9/20/2024 Posts: 8742 Rating: (1168) |
Hello, Are you using latest update? Update 1 for STEP 7 V11 and WinCC V11 Or start a Support Request. Best regards, Wizard |
6/1/2011 4:29 PM | |
Joined: 1/24/2008 Last visit: 5/28/2024 Posts: 30 Rating: (1) |
Hi. Even with the update that you refer (thanks for it) the problem remains. Best regards ML |
6/3/2011 1:57 AM | |
Joined: 1/24/2008 Last visit: 5/28/2024 Posts: 30 Rating: (1) |
Hi. How can I see the instalation languages for V10.5 and V11? My best regards. ML |
6/3/2011 12:03 PM | |
Joined: 9/23/2005 Last visit: 9/19/2024 Posts: 4347 Rating: (1446)
|
Hi, open menu, options, general, User interface language. |
Denilson Pegaia |
|
6/3/2011 6:12 PM | |
Joined: 9/23/2005 Last visit: 9/19/2024 Posts: 4347 Rating: (1446)
|
Witch languages options do you have in both softwares? |
Denilson Pegaia |
|
Follow us on