3/2/2007 1:20 PM | |
Posts: 3149 Rating: (171)
|
Hi which WinCC version are you using? Could you please attache your VB code? nemo |
4/10/2007 7:47 AM | |
Posts: 3 Rating: (0) |
Hallo Nemo, We are using PCS7 6.1 SP1. WinCC version V6.0 SP3a. The VB code I am using is attached in the txt file “ScriptTrend.txt”. In this code there is a line “obj_Trend_Sub1.Start = True” Whit the standard trend control I tried “obj_Trend_Sub1. Activate = True” This did not work because “Activate” is also a VB action! As a work around I made a customized object from the Trend display and renamed the Activate property to Start. This solved the problem and created a new one. The new problem I have is that the Trend print function now longer works. This is because I made a customized object from the tend control. Best regards, Ronny Dortland AttachmentScriptTrend.zip (104 Downloads) |
Follow us on