11/28/2006 1:29 PM | |
Joined: 4/24/2006 Last visit: 5/8/2024 Posts: 8638 Rating: (1151) |
Hello Umesh, Have you seen this faq: http://support.automation.siemens.com/WW/view/en/13396711 There is also mentioned a link about complete deïnstallation of Protool. Best regards, Wizard |
12/1/2006 9:15 AM | |
Joined: 5/8/2006 Last visit: 4/29/2024 Posts: 1085 Rating: (77) |
Hi, maybe you should uninstallProTool completely and then you should install ProTool again without SP3. After the installation youshould try to open your project again. Uninstallation completely include registry entries: http://support.automation.siemens.com/WW/view/de/18697689 Bye... |
12/1/2006 9:41 AM | |
Joined: 4/24/2006 Last visit: 5/8/2024 Posts: 8638 Rating: (1151) |
Hi, Like ZAK mentioned, uninstall Protool completely. But also have a look at the compatibility between Protool and Windows. And system requirements. http://support.automation.siemens.com/WW/view/en/18695605 And the compatibility between Protool and Step7: http://support.automation.siemens.com/WW/view/en/1958565 Best regards, Wizard |
1/24/2010 7:44 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181)
|
Hello, So, Wizard already has been shown compatibility of Windows and Protool. And SP3 of Wondows is out. Try to remove it (How do you uninstall SP3 of Microsoft Windows XP? ). Then uninstall protool (manual delete it from registry) and try to make installation again. Hope this will helps. best regards, Hristo Mihalev |
1/27/2010 8:25 PM | |
Posts: 7 Rating: (0) |
UninstallingSP3 is not an option, since its an windows XP with SP3 integrated. |
Follow us on