Industry Online Support
Technical Forum
4/6/2009 2:32 PM | |
Joined: 3/18/2009 Last visit: 5/6/2024 Posts: 306 Rating: (94) |
Hi Ganesan,
Which version of PCS7 is the existing installation? If I remember correctly, PCS7 v6.1 and above have a very good Web Server option. Webnavigator doesn't support most PCS7 scripts for versions earlier than that.
One of the OS clients, either existing or a dedicated new client can be used for the Web Server. Refer this PCS 7 Web optionmanualfor various configuration options and limitaions. Hope it helps. regards. |
4/7/2009 9:33 AM | |
Joined: 4/5/2006 Last visit: 9/16/2024 Posts: 917 Rating: (63) |
Hi Ganesman, dagasayd well: webnavigator Server has to be installed on WinCC client station, that means need Windows 2003 Server operating system and WebServer license (license depends from how many Webclient you need). Not everything you develop on standard page can be used in web application, you have to look online PCS7 manual to know what function are permitted. dagasayd fine one more: look for which version you need (depending from PCS7 version) Regards |
Follow us on