9/27/2019 3:20 PM | |
Posts: 20 Rating: (0) |
Hello, I've a pulse flowmeter 0-1000 mL/min and K=0.125 pulse/mL. need to configure it. could someone help me doing it. |
9/27/2019 11:45 PM | |
Posts: 20 Rating: (0) |
No I mean how to program it using HSC. I already configured the hardware so as to use I0.0 for the pulses input. |
9/28/2019 1:14 AM | |
Joined: 9/27/2006 Last visit: 9/19/2024 Posts: 12282 Rating: (2684) |
Hello Engea; You do not mention anything about the controller you are using, so it is difficult to answer you properly. There are mamny posts on this forum on the subject that you might look at, such as: https://support.industry.siemens.com/tf//ww/en/posts/flow-meter-input/131064?page=0&pageSize=10 Hope this helps, Daniel Chartier |
9/28/2019 4:30 PM | |
Joined: 9/27/2006 Last visit: 9/19/2024 Posts: 12282 Rating: (2684) |
Hello Engea; Have a look at this Application Example for S7-1200 HSCs: S7-1200: Application Examples for High-Speed Counters (HSC) https://support.industry.siemens.com/cs/ww/en/view/109742346 With these samples and the HSC instruction descriptions you should be able to work your project out. I have extracted the HSC section of the Technological functions of the S7-1200, from the following system manual: SIMATIC S7 S7-1200 Programmable controller https://support.industry.siemens.com/cs/ww/en/view/109759862 You will find them as an attchment below. Hope this helps, Daniel Chartier Attachments71200_system_manual_HSC functions.pdf (270 Downloads) |
9/28/2019 5:53 PM | |
Posts: 20 Rating: (0) |
i think i could use the frequency function so as to calculate number of pulses per second then calculate the flow, |
Follow us on