4/5/2021 11:35 AM | |
Joined: 10/1/2018 Last visit: 7/10/2022 Posts: 66 Rating: (0) |
Yes, I need to get the difference in values between the value in this cycle and in the previous cycle. |
4/5/2021 9:16 PM | |
Joined: 10/1/2018 Last visit: 7/10/2022 Posts: 66 Rating: (0) |
I was amazed that the analog-to-digital conversion takes 300 or 50ms. Is this your measurements or data from a datasheet? I made a block to delay the analog signal, but I did not like that the signal at the output stays too long after decreasing the value at the input. And I made a faster circuit. Results in the attached file. Suddenly someone else will come in handy. AttachmentIncrease test.zip (196 Downloads) |
4/6/2021 1:29 AM | |
Joined: 10/1/2018 Last visit: 7/10/2022 Posts: 66 Rating: (0) |
I really often over complicate the solution of the problem. Thanks for the simple solution) I think in this case it is justified, since it is a solution to a more general problem of determining the rate of change of a value.
AttachmentIncrease test 2.zip (226 Downloads) |
Follow us on