1/29/2015 2:41 PM | |
Posts: 1058 Rating: (93) |
I guess it should be possible for your motor, as DC/DC/DC outputs are capable of driving up to 0.5 A with a max. load of 5W. Look here for detailsfor your CPU: SIMATIC S7 S7-1200 Programmable controller You should also read this: TIP for S7-1200 und PWM SIMATIC STEP 7 S7-1200 Motion Control V13 SP1 regards |
This contribution was helpful to1 thankful Users |
Follow us on