Industry Online Support
Technical Forum
12/12/2010 3:40 AM | |
Posts: 2964 Rating: (482)
|
Hi NIt.... Good Morning.... If all axis is properly Optimized he can get the result...... Regards, Ekalavya |
12/14/2010 10:34 AM | |
Posts: 11 Rating: (0) |
I checked the parameter, it was 0.1, so I changed it to 0.05, but It seems there's nothing changed. I changed #36500 only for Y axis, right? or, should I have changed other axes as well? I let them be 0.1 as before for X & Z axes. then I noted some fishy thingsin my machine: 1- the backlash has changed since 2 weeks ago that I set, yesterday I checked andit was 0.4 (0.07 increased!!) 2- there is impact at the reversingdirectionof Y axis, when I give it a repeating back and forthmovemnet, there is a significant impact at the reverse point, also I found out that this impact exists when I change the speed (by pressing "rapid" button in jog mode) at the same direction of Y axis movement. I took a video for back and forth state, it is not so good, but may help I worry so much about the machine, I think it is going out of control whats wrong?! AttachmentVIDEO_033 shock impact.zip (179 Downloads) |
Follow us on