8/26/2013 7:18 AM | |
Joined: 6/15/2010 Last visit: 2/18/2021 Posts: 31 Rating: (1) |
Dear experts, Please note that I’m considering ET-200M with redundant power supplies in S7-412H configuration and I’ve a few questions on AI & DI cards. Can someone please advise what are the wiring connection details · at terminal 1/11 and 21/40 for 6ES7321-1CH00-0AA0 (16 CH DI module). Will it need to be +24Vdc and 0Vdc respectively? · at terminal 1/21 and 20/40 for 6ES7321-1CH00-0AA0 (16 CH DI module). Will it need to be +24Vdc and 0Vdc respectively? Attached manual doesn’t show this. Attachment6ES7331-7NF10-0AB0 AI.pdf (37 Downloads) |
8/26/2013 7:37 AM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (711)
|
Hello, The 6ES7321-1CH00-0AA0 input module does not need 24V, see attached diagram. regards, Marcjan Attachment6ES7321-1CH00-0AA0.pdf (40 Downloads) |
Problem solved? |
|
This contribution was helpful to1 thankful Users |
Follow us on