6/15/2010 12:02 PM | |
Posts: 122 Rating: (1) |
Hi everyone, I wanted to use one of this methods (set/reset bit) in my network, which consists of an S7-300 and several HMI devices. My question might be easy to anwser for you guys, but I'm new in this and it's the first time I'm learning about Profibus. I know about the "token" connection mode in Profibus and my question is: if the PLC is communication with Panel2 and I have a momentary bit set in Panel 3 which will be inmediately reset using one the methods above, what happens to that information? Does it get lost? Is it necessary for the PLC to be communicating with the Panel in the exact moment in which the bit is set? Thanks for your patience, Sara Splitted from Momentary tag using button. |
Last edited by: O_Moderator at: 6/15/2010 12:52 PMnew subject after splitting |
|
6/15/2010 4:01 PM | |
Joined: 4/29/2010 Last visit: 3/19/2024 Posts: 1557 Rating: (161)
|
Hello, no it doesn`t go lost. The panel communicate with the plc in every cycle. best regards |
6/16/2010 4:06 PM | |
Posts: 122 Rating: (1) |
I undestand what you do there. I think I could make it work in my case too. Thanks you so much for the help Sara |
6/18/2010 1:30 PM | |
Posts: 122 Rating: (1) |
Thanks Skimmer! You solved two doubts in one reply I will try to do what you say too Sara |
6/18/2010 3:02 PM | |
Posts: 122 Rating: (1) |
No problem Darius. I will try both solutions and come here with the results. Sara |
Follow us on