2/9/2010 7:09 PM | |
Posts: 12 Rating: (0) |
Hi again, I found this really usefull and clarifying /tf/WW/en/Posts/38403 Besides,according to online help,(I undestood that) downloading to PLCSIM does affect my POs. Is it correct? Thanks againg |
2/12/2010 9:07 AM | |
Joined: 4/5/2006 Last visit: 3/13/2024 Posts: 917 Rating: (63) |
Hi OsRel , downloading AS program in PLCSIM doesn't book PO. ffollow your link postaed above, then Phantom75link, at the end follow the last link 27002752. Display or download document and search for "PLCSIM" or go to chapter : What you should know about CFC -> Count and Booking of the PO Licenses there answer to your question hope can help regards |
2/18/2010 10:18 PM | |
Joined: 3/14/2008 Last visit: 4/18/2024 Posts: 2064 Rating: (926) |
I don't think the documents will help him.. I to had the same thing.... I have a full license of PO, but when downloading my program to PLCsim, I got a message that there weren't any PO available. The documents will describe how the PO will work, but maybe there is a glitch when you want to download to PLC sim... or at least, confuse the user. The PO are not being abstracted from your license when using plcsim.. Best regards... |
If I could help you, you can use the RATE button. Thank you. |
|
2/19/2010 1:30 PM | |
Joined: 4/5/2006 Last visit: 3/13/2024 Posts: 917 Rating: (63) |
Hi Oreca ,
that's no correct: sownloading program into PLCs doesn't book license. about previuos post: messages says progarm is registrered on other CPU and so on.... you have to use "download for test" function. This function permit you to download same program on a different CPU without booking license again. Press help button in download popup windows during program download: a good explanation about testsame program over a different CPU. hope can help regard |
2/19/2010 7:58 PM | |
Joined: 3/14/2008 Last visit: 4/18/2024 Posts: 2064 Rating: (926) |
Hello Cbo, Yeah I now the function, but I remember I got the same message as the topic creator, showing me that I didn't have any license available, but I did have them. I also used first the download program function and indeed when using the test function,. there were nowarnings again. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on