11/19/2010 1:36 PM | |
Joined: 11/14/2008 Last visit: 5/6/2024 Posts: 504 Rating: (22) |
Difference between F and H is that , F is more for safety applications and H for more fault-tolerant systems... Also see pdf pls... AttachmentS7_400_h_en_en-US.zip (236 Downloads) |
11/22/2010 8:00 PM | |
Joined: 7/2/2008 Last visit: 4/5/2024 Posts: 928 Rating: (306)
|
Hello PCI,
It falls in the FH category.
I give your colleagues all the respect but one of the 1st things I've learntwhen I was starting my career is to trust what I readand respect whatI hear. The term Process Safety is good no doubt however the name that's used by all technology providers and engineering houses is SIS (Safetyinstrumented system). The name SIS is used to describe any ESD (Emergency shut down) or PSD (Process shut down) system. In Siemens world as you could see we have the F/FH categories which is as stated by dmertensis mainly used to cover SIS applications. I think you will find thislink very useful. It has 2 main links, one for distributed safety (Factory automation) and the other isSafety Integrated for the Process Automation in which you can read and learn many things. Normally,an SISis controlled by a special PLC that has nothing to do with process control (PID loops). The main task of this PLC is to handle the safety logic of the plant. This fail safe PLC communicates with process controller (DCS) through a gateway. It's alwayslittle hard to find both DCS and ESD systems coming from a single vendor and even if you can get them from a single technology provider, it's still hard for both to share the same engineering tools. Now SIEMENS put both the fail safe PLC (F or FH) and the process controller (S7-400 or 400H) under the PCS7 which means simplified engineering and easy integration. Moreover, both process control and SIS can be integrated ina single controller which is your case since you have standard and fail safe modules combined together. This is well shown in Integrated Control + Safety. So, based on this link we can create a new category for your system and call it common FH .
That's a tough question to answer. This might not be the perfect answer and just represents my own opinion. 1st of all the most important thing for a fail safe system is the certificate. And the important thing in the certificate is which standards have been taken into consideration while issuing the certificate. Both distributed safety and F-systems are mainly based on IEC61508. Then distributed safety which is more related to safety of machinery (Factory automation) is more based on IEC62061. The F-system which is more related to process safety is more based on IEC61511. There are 2 certificates now, one for distributed safety (check report)and the other is the F/FH certificate (check report). You can find that both had taken into consideration the IEC61511. The 416F has been mentioned in thereport of the distributed safety (Machinery) and was not mentioned in the S7-F/FH (Process) report which means it's not tested with the S7-F library blocks. For example, you can't use safety matrix with 416F because 1st Siemens doesn't support it and 2nd this solution will not be TUV certified. You can also check the area of application of S7-400 fail safe CPUs here where you will not find the word process mentioned I hope I answered your question. Best regards, H-H |
Last edited by: H-H at: 11/23/2010 12:29 AMLast edited by: H-H at: 11/23/2010 12:20 AM |
|
This contribution was helpful to2 thankful Users |
11/23/2010 12:39 AM | |
Joined: 7/2/2008 Last visit: 4/5/2024 Posts: 928 Rating: (306)
|
Dear dmertens, I really like what you have written. I just have some comments. I don't know why Siemens didn't put the latest reportof certificate inthispage. Anyhow, the latest report can be found here in which you can see that the 412-3H has been included to give it the title F so it becomes 412-3FH. It's little bit confusing but the burner management system blocks can be used in both distributed safety and S7-F library. Where can you find an overview of the "Fuel Technology" function blocks for fail-safe automation systems? Best regards, H-H |
11/23/2010 8:13 AM | |
Posts: 2 Rating: (0) |
Thanks you all, information here should be enough for me to fully understand what it means. |
Follow us on