Industry Online Support
Technical Forum
2/19/2008 4:13 PM | |
Joined: 3/29/2006 Last visit: 5/29/2017 Posts: 151 Rating: (8) |
Just a simple example. Please refer to Compendium Masterdrives MC, chap 8.3 and functiondiagrams 150 and 160. Sending: K0751.01 = K0001 (100 %) K0751.02 = K0002(200 %) K0751.03 = K0003(-100 %) K0751.04 = K0004 (-200 %) Receiving P749.01 = 0.0 P749.02 = 0.1 and you will see r750.01 = 4000 h (100 %) r750.02 = 7FFF h (200 %) r750.03 = C000 h (-100 %) r750.04 = 8000 h (-200 %) Now you can use this values in the drive via connectors K7001 to K7004. ------------------------- http://support.automation.siemens.com/WW/view/en/23660019 |