4/4/2010 9:57 AM | |
Posts: 352 Rating: (7) |
Hello You could always check out the Office Chart Component installed with MS Office. This could might do the trick, but I think it require some programming. I Also think there are other 3rd parity components available on the internet. The problem might me that the client must be installed on each client if you are running av multi user environment. I found this one as an example but I have never tested it http://www.nevron.com/Gallery.ChartForActiveX.RadarChartsGallery.aspx O |
Last edited by: GoForIT at: 4/4/2010 10:15 AM |
|
This contribution was helpful to1 thankful Users |
4/5/2010 5:54 PM | |
Joined: 8/11/2008 Last visit: 4/8/2024 Posts: 67 Rating: (22) |
you can use standard wincc objects also. i attached an example i did in some minutes, so, don't expect code optimization even though, it's working fine, and if you have any doubt, please let me know. best regards ------------------------------------------------------------------------------- a reviewed script is available just a few posts later.
AttachmentRadarPlot.zip (445 Downloads) |
Last edited by: rogermann at: 4/6/2010 10:00 PMinform about new version Roger A. Manrique |
|
4/6/2010 8:24 PM | |
Joined: 8/11/2008 Last visit: 4/8/2024 Posts: 67 Rating: (22) |
ok, folks as promissed, RadarPlot project with a better (and full commented) script hope you like it. best regards
AttachmentRadarPlot_V2.zip (521 Downloads) |
Roger A. Manrique |
|
This contribution was helpful to4 thankful Users |
12/25/2018 12:02 PM | |
Posts: 4 Rating: (0) |
Hi Guys This is indeed an interesting one. Do you think it would be possible in new TIA? |
1/12/2019 5:18 PM | |
Posts: 55 Rating: (1) |
I would also be interested in using this in TIA is it possible? |
Follow us on