4/29/2009 9:16 AM | |
Joined: 7/2/2008 Last visit: 8/26/2024 Posts: 928 Rating: (308) |
HelloOZI, Please check this thread Best regards. H-H |
4/29/2009 9:24 AM | |
Joined: 9/27/2006 Last visit: 9/18/2024 Posts: 12282 Rating: (2684)
|
Hello osi; From the FAQ; “S7-400 memory concept” If you have a flash memory card plugged in, transfer blocks to the external load memory with "PLC >Load user program onto memory card". However, in the case of "PLC >Load user program onto memory card", the CPU has to be set to STOP mode first before the user program can be transferred. http://support.automation.siemens.com/WW/view/en/7302549 Hope this helps, Daniel Chartier |
This contribution was helpful to2 thankful Users |
Follow us on