(0)| 8/29/2019 10:02 AM | |
|
Posts: 1 Rating:
|
Hello, Currently we are trying to ramp an analog output as smoothly as possible within 1 or 2 seconds for use with a hydraulic proportional valve, currently were using this ramp FB, however this ramp block is not smooth enough as you can see the handles on the valve stutter whilst moving because the steps the ramp block sends out are too big. The ideal situation would be that we the analog output simply ramps up and down consistantly with no steps. Is there some kind of output module or serparate component after the output that could do this for us? Our preference would be 0..10V for easy of measuring, but other solutions are always welcome. Were currently using a 6AG1510-1SJ01-2AB0, ET200SP with a 6AG1510-1SJ01-2AB0 analog output. Many thanks, Rik. |
Last edited by: Jen_Moderator at: 08/29/2019 11:27:03Optimized link. |
|
| 8/29/2019 1:33 PM | |
|
Joined: 9/23/2005 Last visit: 12/22/2025 Posts: 5147 Rating:
|
I can't see anything, sorry. Where do you call the FB (which OB)? What is the scan time of this OB? BTW, the output card's product code is invalid. |
|
Regards, |
|
| 8/29/2019 4:07 PM | |
|
Joined: 7/7/2010 Last visit: 12/23/2025 Posts: 16323 Rating:
|
If your hydraulic proportional valve has configurable parameters, like ramp rate, control input type (+/- 10V, 4-20mA, 0-20mA, +/- 5V, etc), select one that your analog output module supports natively. It also sounds like your plc scan time is long. You may consider creating a cyclic interrupt OB that runs every 2 ms that handles the ramp control. The ramp output would drive the output tagname with :P appended to the name so it changes the analog output immediately rather than at the end of the current OB1 scan. ex: output tag name out_Valve_Control ---> out_Valve_Control:P
|
|
science guy |
|
Follow us on